Eclipse-based plug-in on Mac OS X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Eclipse-based plug-in on Mac OS X

4,230 次查看
cardoso
Contributor II

Anyone get this working on Mac OS X?

I follow the installation instructions but after the installation, it raise an error message:

An internal error occurred during: “Open last Processor Expert project”.

java.lang.NullPointerException

And in the log file:

!ENTRY com.freescale.processorexpert.core 4 0 2013-09-07 01:45:19.428
!MESSAGE reg.getExtensionPoint is empty

!ENTRY com.freescale.processorexpert.core 4 0 2013-09-07 01:45:19.531
!MESSAGE No com.freescale.processorexpert.core.PEservice extension found!

!ENTRY com.processorexpert.core.ide.wizard.ui 2 0 2013-09-07 01:45:29.810
!MESSAGE External elements location /Applications/eclipse/ProcessorExpert/Config/PE/CPE/wizard_data/wizards/components does not exist

Thanks

6 回复数

3,652 次查看
maxpiepenbrink
Contributor II

I was able to set up Processor Expert ("Driver Suite") in OSX with just stock Eclipse Kepler. It takes some extra setup time but it works.

3,652 次查看
krekeltronics
Contributor II

Any progress on this? I have a pretty nice Kepler installation going to stay in OS X. It will be cool to see if Processor Expert might be usable as well!

Cheers,

Patrick

0 项奖励
回复

3,652 次查看
liborukropec
NXP Employee
NXP Employee

Hello,

Driver Suite 10.5 will support MAC OS; it should be available by the end of this year. The upcoming Driver Suite 10.4.1 Update will have better support for MAC OS even it is not officially supported yet.

Best regards,

Libor Ukropec

Processor Expert Team

0 项奖励
回复

3,652 次查看
vfilip
NXP Employee
NXP Employee

Hello,

this is currently not supported and as far as I know that there is no plan to support PEx plugins for MAC in near future. However I have passed this request to our management.

Best regards

Vojtech Filip

Processor Expert Support Team

3,652 次查看
ghemstreet
Contributor II

Which Processor Expert product are you trying to install? QCS, Driver Suite or Component Development Environment?


0 项奖励
回复

3,652 次查看
cardoso
Contributor II

I'm trying to install the Driver Suite 10.2

0 项奖励
回复