Easy Importing of K60 pin assignments in Component Inspector?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Easy Importing of K60 pin assignments in Component Inspector?

Jump to solution
1,451 Views
rc
Contributor I

I'm new to using CodeWarrior PE and am trying to configure my K60 pin/resource assignments using the component inspector. Is there an easier way to assign pin names and resources, or does each pin have to be added manually? I'm thinking there is perhaps a way to import a text or pin file similar to an FPGA?

I haven't found much on this topic in the forums or CW help files but I'm thinking there must be an easier way than assigning each of these resources (and changing them when needed) individually?

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,328 Views
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, that would be a useful thing (to apply settings to a component in the project). As of MCU10.2, this is not supported yet.

But you can at least copy existing settings/components which might be helpful for you too:

http://mcuoneclipse.wordpress.com/2012/05/04/copy-my-component-settings-processor-expert-templates/

 

Hope this helps,

BK

View solution in original post

0 Kudos
Reply
1 Reply
1,329 Views
BlackNight
NXP Employee
NXP Employee

Hello,

Yes, that would be a useful thing (to apply settings to a component in the project). As of MCU10.2, this is not supported yet.

But you can at least copy existing settings/components which might be helpful for you too:

http://mcuoneclipse.wordpress.com/2012/05/04/copy-my-component-settings-processor-expert-templates/

 

Hope this helps,

BK

0 Kudos
Reply