Does processor expert support xgate code generation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does processor expert support xgate code generation?

1,099件の閲覧回数
yitzchak
Contributor I

I think the answer is no; but I can find little to nothing about it.

0 件の賞賛
返信
1 返信

962件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

processor expert/Device initialization does not support any code generation for XGate.

We say “processor expert does not support any code generation for XGate”, for instance, processor expert can not be able to generate a prm file that include XGate associated content. So user has to rewrite their own xgate supporting prm file but can’t use pe generated prm.

Another example is that pe also can not generate xgate supported vector table, etc.

thus it loose some of the major advantages of pe.

This is the reason that if you make a project with XGATE the Proc.Exp. and Device initialization/processor expert option isn't enabled.

in practice, we don’t recommend user use processor expert and xgate together in one project.  we only have sample code that use xgate or  pe only but never use them together.

If you want take use of the processor expert tool generated code, please create pe project for generated the related driver code. then port the associated code to your xgate project.

0 件の賞賛
返信