Does development board MCIMX8M-EVKB support ublox's WI-FI module M2-JODY-W3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does development board MCIMX8M-EVKB support ublox's WI-FI module M2-JODY-W3?

1,294 次查看
SoniaLuo
Contributor I

Hi guys,

We currently have MCIMX8M-EVKB and want to evaluate the ublox's WI-FI card M2-JODY-W3 of NXP Q9098 chip.

Does the board support the module?

Can the card directly be plugged into the M.2 E interface?

Which online repository can we use to build an image for MCIMX8M-EVKB with the driver to support M2-JODY-W3?

 

Thank you in advance.

Sonia

0 项奖励
回复
1 回复

1,267 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @SoniaLuo 

88W9098 | 2x2 Wi-Fi® 6 Bluetooth 5.3 for IoT | NXP | NXP Semiconductors, the link from which shows that supports the Module.

Regarding the drivers, there should be available in default BSP.

 

Best regards

Harvey

0 项奖励
回复