Does development board MCIMX8M-EVKB support ublox's WI-FI module M2-JODY-W3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does development board MCIMX8M-EVKB support ublox's WI-FI module M2-JODY-W3?

1,285 Views
SoniaLuo
Contributor I

Hi guys,

We currently have MCIMX8M-EVKB and want to evaluate the ublox's WI-FI card M2-JODY-W3 of NXP Q9098 chip.

Does the board support the module?

Can the card directly be plugged into the M.2 E interface?

Which online repository can we use to build an image for MCIMX8M-EVKB with the driver to support M2-JODY-W3?

 

Thank you in advance.

Sonia

0 Kudos
Reply
1 Reply

1,258 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @SoniaLuo 

88W9098 | 2x2 Wi-Fi® 6 Bluetooth 5.3 for IoT | NXP | NXP Semiconductors, the link from which shows that supports the Module.

Regarding the drivers, there should be available in default BSP.

 

Best regards

Harvey

0 Kudos
Reply