DeviceDataPtr in ResetCounter and similar methods

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DeviceDataPtr in ResetCounter and similar methods

ソリューションへジャンプ
4,090件の閲覧回数
luisgallegos
Contributor III

Hello.

I am using the TimerUnit_LDD and I enabled the ResetCounter method to generate it's code. I then dragged the ResetCounter method from the Component window on the right, on the drop-down list of the TimerUnit_LDD, to insert it in my code. This generated the following code:

     ComponentName_ResetCounter();

With no arguments. However, when I try to build my code it returns the error "too few arguments to function ComponentName_ResetCounter". Hovering over the method in the Component Inspector, I see that this function requires the argument "LDD_TDeviceData *DeviceDataPtr" and that it is a "Device data structure pointer returned by Init method". However, looking through the code I can't seem to find what this data pointer value is.

I know this is a simple method which I could do on my own just assigning a 0 to the CNT register, but this data pointer seems to be necessary for other more complicated methods.

Does anyone have some reference as to what this pointer is?

Also, how can the EventMask values be set and used?

I am new to Processor Expert, so these are probably very basic questions.

Thanks.

ラベル(1)
1 解決策
3,692件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

you can find more details on method usage in the component´s help or in FSL info-center web:

Freescale Technical Information Center

Another way, that is not mentioned in the help, could be usage of the DeviceDataPtr defined in the component´s header file if Autoinitialization property is set to yes.

best regards

Vojtech Filip

Processor Expert Support Team

元の投稿で解決策を見る

4 返答(返信)
3,692件の閲覧回数
luisgallegos
Contributor III

Hello.

Thanks for the reference.

Guess I wasn't looking close enough and missed that.

Thanks again.

0 件の賞賛
返信
3,693件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

you can find more details on method usage in the component´s help or in FSL info-center web:

Freescale Technical Information Center

Another way, that is not mentioned in the help, could be usage of the DeviceDataPtr defined in the component´s header file if Autoinitialization property is set to yes.

best regards

Vojtech Filip

Processor Expert Support Team

3,692件の閲覧回数
kiven
Contributor II

Hello,

I have the same problem that Luis had, but I just cant figure out whats going on with my code.

Im using a TimerUnit to make 2 PWM signals, one on each channel (0 & 1), and I want to change the offset values by using SetOffsetTicks method.

My code is this one:

TU2_SetOffsetTicks(LDD_TDeviceData *DeviceDataPtr, uint8_t 0, TU2_TValueType 25000);

cause it didn't work I tried with this one:

TU2_SetOffsetTicks( LDD_TDeviceData *TU2_TDeviceDataPtr, uint8_t 0, TU2_TValueType 25000);

The errors that I get are these ones:

../Sources/Events.c: In function 'AS1_OnRxChar':  //*****************Im trying to use this method (SetOffsetTicks) inside this Serial communication event but even if I try to use it in the main code I still get this.

../Sources/Events.c:101:26: error: expected expression before 'LDD_TDeviceData'

mingw32-make: *** [Sources/Events.o] Error 1

I have Auto initialization enabled.

How do I fix this?

Thanks in advance.

0 件の賞賛
返信
3,692件の閲覧回数
Petr_H
NXP Employee
NXP Employee

You seem to have incorrect syntax of the function call. The function needs to be called without the parameter type names.

Like this:

TU2_SetOffsetTicks(TU2_DeviceData, 0, 25000);

best regards

Petr Hradsky

Processor Expert Support Team