Configuring OPWM using EMIOS on MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Configuring OPWM using EMIOS on MPC5777C

跳至解决方案
2,896 次查看
ikarkala
Contributor III

Hi,

 

I am trying to configure an EMIOS channel in OPWM mode . I wanted to know if there is a way to configure it for a fixed amount of time . Example : configuring it in at 5Mhz frequency for 4 seconds ?

Regards,

Indy

0 项奖励
回复
1 解答
2,863 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no such mode is supported by HW in single channel. Output disable  (ODIS) feature can be used, when flag of another channel can disable channel output. Thus another channel can count that 4sec delay and after that disable PWM output of channel with ODIS enabled (but PWM still run).
Or you need to use SW way to stop PWM channel.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,864 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no such mode is supported by HW in single channel. Output disable  (ODIS) feature can be used, when flag of another channel can disable channel output. Thus another channel can count that 4sec delay and after that disable PWM output of channel with ODIS enabled (but PWM still run).
Or you need to use SW way to stop PWM channel.

BR, Petr

0 项奖励
回复
2,858 次查看
ikarkala
Contributor III
Thank you
0 项奖励
回复