CW10, Processor Expert generates duplicate code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10, Processor Expert generates duplicate code

2,723件の閲覧回数
Nik
Contributor III

With licensed CW, MC9S08AC60

For example, PE generates:

void TPM10_1_MS_TIMER_OnInterrupt(void) {
 /* Write your code here ... */
}

I then add code.  I add another bean, and PE adds another copy of the above.

Anyone else have this problem or know the solution?

Thanks,

-Robern

0 件の賞賛
返信
4 返答(返信)

2,548件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

Could you please create a project that demonstrates your problem exactly and post it here? I am not aware of such problems in CW V10.

 

best regards
Vojtech Filip
Processor Expert Support Team

0 件の賞賛
返信

2,548件の閲覧回数
paulsawyer
Contributor I

I have the same issue with duplicate code.  If I leave the "/* Write your code here */" in the code, then the function is not duplicated.  Sketchy but true.

0 件の賞賛
返信

2,548件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

could you please provide step by step process how to reproduce it? Are you able to reproduce it also in CW V10.4?

I am not able reproduce it...

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信

2,548件の閲覧回数
paulsawyer
Contributor I

It is with CodeWarrior v10.4. In my project’s Sources\Events.c file, function SM1_OnBlockSent(), I deleted the comment ‘/*Write your code here … */’ and added my own code. In CW, when I selected to Generate Processor Expert Code, the Events.c file was recreated. It had my SM1_OnBlockSent() file as it was with my code, but there was a new SM1_OnBlockSent() file at the end.

However, when I tried to recreate it with the same original Events.c file, it works properly. I also tried changing other functions in this file, but it still works properly.

Paul Sawyer | Senior Design Engineer | Nuvation Research Corp, Canada | 519-746-2304 ext 2259

0 件の賞賛
返信