CLCR663 code for DESELECT function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CLCR663 code for DESELECT function

跳至解决方案
2,630 次查看
K_Salewicz
Contributor II
Can you evaluate why the following code for DESELECT function does not work ?
 
/* Deselect and switch off NFC RF field according
   ISO/IEC 14443-4 B.2.3 Scenario 3 DESELECT
   Comment Block No. (0) PCD PICC Block No. (1) Comment
   1. rule 1 I(0)0 ===> 0 rule D
   2. rule B 1 <=== I(0)0 rule 10
   3. S(DESELECT) request ===>
   4. <=== S(DESELECT) response rule 3
   i-block is decoded in  respnse trailer (sw1 sw2)
*/
export void NXP_NFC_Deselect()
{
  /* I-Block */
  NFC_WriteRegister3(NXP_REG_FIFODATA, 0x43, 0x00); // I(chaining 0) block=0, SW1+SW2: 01000011 
  NFC_ReadRegister3(NXP_REG_FIFODATA, 0x01, 0x00);  // (00xxxxxx)b (not (00xxx101)b
 
  /* S-Block(DESELECT) request, PCB 11000010b (CID 0), CID & NAD (optional fields), EDC (2 bytes, switched off) no INF field */
  NFC_WriteRegister2(NXP_REG_FIFODATA, 0xc2);
 
  /* ~4,8 ms max deactivation frame waiting time */
  delay_ms(2);
 
  /* S-Block(DESELECT) response */
  if (!NFC_ReadRegister1(NXP_REG_FIFODATA, 0xc2)) // TODO supervisory 0001b
  {
    /* ~4,8 ms max deactivation frame waiting time */
    delay_ms(2);
  
    /* FIXMP Rule 8. If the S(DESELECT) request is not answered by an error-free S(DESELECT) response the S(DESELECT) request may be re-transmitted or the PICC may be ignored. */
    NFC_ReadRegister1(NXP_REG_FIFODATA, 0xc2)
  }    
 
  /* Disable NFC RF field */
  NXP_NFC_RF_FIELD_OFF();
}
 
export void NXP_NFC_RF_FIELD_OFF()
{
  /* switch RF field OFF */
  NFC_Array_Write[0] = 0x86U;
  NXP_NFC_WriteRegister(NXP_REG_DRVMODE, NFC_Array_Write, 0x01);
}
 
u8 NXP_NFC_ATQA()
{
  /* Receive 16 bit ATQA */
  if(2 != NFC_Array_Read[0U])
  {
    return NFC_APDU_ATQA_SIZE_ERROR;
  }
 
  /* bit 6, 13-16 is 0 */  
  if ((0x00 != (NFC_Array_Read[1U] && 0x20)) ||
      (0x00 != (NFC_Array_Read[1U] && 0xF0)))
  {
    return NFC_APDU_ATQA_RFU_ERROR;
  }
  
  // FIXMP check further parameters
  return TRUE;
}
0 项奖励
回复
1 解答
2,584 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @K_Salewicz 

Please refer to sw6693 to implement your application. sw6693 is an open source routine, please go to the NXP website to download.

Best Regards,

kelly

在原帖中查看解决方案

2 回复数
2,577 次查看
K_Salewicz
Contributor II

Thank you very much, Kelly !

0 项奖励
回复
2,585 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @K_Salewicz 

Please refer to sw6693 to implement your application. sw6693 is an open source routine, please go to the NXP website to download.

Best Regards,

kelly