CAN_LDD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN_LDD

1,529 次查看
markbishop
Contributor I

I am trying to get a CAN_LDD interface working on a MK60FX512 and I am noticing that the SYNCH bit in ESR1 of the Flexcan module is set, meaning that the "FlexCAN is not synchronized to the CAN bus."

I can only assume that this is why when I send data from the micro to another device, that the data doesn't come across. 

I am using the "Sending data frame with interrupt service" example provided in the documentation and the CAN1_OnFreeTxBuffer is never hit on a break point.

Also, is it correct that I would be seeing pulses on the CAN bus if I am not actively sending data?  I don't recall from the standard if there is continual packets for timing being transmitted.

0 项奖励
回复
1 回复

1,294 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mark,

-  "the SYNCH bit in ESR1 of the Flexcan module is set", this meaning FlexCAN is synchronized to the CAN bus.

pastedImage_0.png

- And pastedImage_1.png , could you please tell me which DOC ?

And also do you meaning when you test the example you mentioned , it can not work well ? If yes,

please tell me which , i can check on my side .

You can also describe your problem in detail .

Hope it helps

Alice

0 项奖励
回复