CAN_LDD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN_LDD

1,541件の閲覧回数
markbishop
Contributor I

I am trying to get a CAN_LDD interface working on a MK60FX512 and I am noticing that the SYNCH bit in ESR1 of the Flexcan module is set, meaning that the "FlexCAN is not synchronized to the CAN bus."

I can only assume that this is why when I send data from the micro to another device, that the data doesn't come across. 

I am using the "Sending data frame with interrupt service" example provided in the documentation and the CAN1_OnFreeTxBuffer is never hit on a break point.

Also, is it correct that I would be seeing pulses on the CAN bus if I am not actively sending data?  I don't recall from the standard if there is continual packets for timing being transmitted.

0 件の賞賛
返信
1 返信

1,306件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mark,

-  "the SYNCH bit in ESR1 of the Flexcan module is set", this meaning FlexCAN is synchronized to the CAN bus.

pastedImage_0.png

- And pastedImage_1.png , could you please tell me which DOC ?

And also do you meaning when you test the example you mentioned , it can not work well ? If yes,

please tell me which , i can check on my side .

You can also describe your problem in detail .

Hope it helps

Alice

0 件の賞賛
返信