CAN_LDD, how to use ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN_LDD, how to use ?

5,374 次查看
kentachang
Contributor I

Hello,

I hope to use CAN_LDD for CAN bus transceiver, but I do not know How to setting the CAN_LDD component?

attachment is my project, please let me know ...

 

Best Regards,

Kenta 

Original Attachment has been moved to: _K60_DN512__CAN_LDD.rar

0 项奖励
回复
3 回复数

4,721 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Kenta,

I think you can refer CAN_LDD sample code under {CW10.6 install}\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K60N512\CAN

====================================

this answer is for you. if it helps,please click on "correct answer" button. thanks!

Best Regards.

ZhangJun

4,720 次查看
kentachang
Contributor I

Hi Jennie,

I see the TWR-K60N512/CAN example project and  modify my project(attached). I want to let CAN0 module to repeat transmit messages and receive messages.

Can you help me to modify or correct my project? Let it to send messages and read messages.

Best regards,

Kenta

0 项奖励
回复

4,718 次查看
kentachang
Contributor I

Hi Jennie,

I find a circuit on the page 200 AN2865 is good for me.

Is there a MK60 example code like AN2865 ?

and What value is the resistor ?  the power supply will be 3.3V not 5.0V

please ...

Kenta  

0 项奖励
回复