Build on PEx-generated code fails: EventCntr16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build on PEx-generated code fails: EventCntr16

ソリューションへジャンプ
11,433件の閲覧回数
Smiffytech
Contributor III

Working with Codewarrior 10.2, MC9S08AC16CFG.

I add the component EventCntr16, with mode Repetitive and Iterations before action 32768. My goal is to count pulses on a pin, and invoke EC161_OnEnd every time the count is reached. (I'm assuming that the counter is cleared automatically - or do I have to do this manually as part of EC161_OnEnd?)

When I go to build project, I get the following error:

DescriptionResourcePathLocationType
C5200 Limits.h file not foundEC161.c/nebinclock/Generated_Codeline 48C/C++ Problem
make: *** [Generated_Code/EC161_c.obj] Error 1nebinclockC/C++ Problem

What am I - or is PEx - doing wrong?

ラベル(1)
0 件の賞賛
返信
1 解決策
11,187件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

yes, this location is correct. Could you please try to change the include from #include <Limits.h> to #include <limits.h> and try to build the project again? I assume it should help because you are running under Linux.

best regards

Vojtech Filip

Processor Expert Support Team


元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
11,183件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

could you please post here some simple project in order to reproduce it on our side? Could you please also try to create the same in CW V10.3 (if possible)? Did you try clean the project? The issue might also by in upper/lower L letter Limits.h/limits.h.

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信
11,183件の閲覧回数
Smiffytech
Contributor III

I can confirm that the problem persists even if I create a new project and add only the EventCntr16, configured as I mentioned, and attempt to build. (This is also on a different computer.)

The 10.2 system is running on my regular machines - Linux laptop & desktop. I only have 10.3 beta on a Windows VM - where I am unable to reproduce the problem. (Although 10.3 won't allow me to choose the CFG package, only CFD, if that means anything.)

What files do you want me to post, or is there a way to export the configuration?

0 件の賞賛
返信
11,183件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

Could you please also check that the Limits.h is on disk in correct form corresponding value in include #include <limits.h>?

Regarding Export: The whole project would be the best.

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信
11,182件の閲覧回数
Smiffytech
Contributor III

Not sure where I should look for limits.h, but it's not there in the project directory. Looking in the actual CW installation directory, this is the only one that looks relevant:


./CodeWarrior_MCU_10.2/MCU/lib/hc08c/include/limits.h (size 7909 bytes)

Please find attached zip file of my 'test' directory.

Thanks!

0 件の賞賛
返信
11,188件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

yes, this location is correct. Could you please try to change the include from #include <Limits.h> to #include <limits.h> and try to build the project again? I assume it should help because you are running under Linux.

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信
11,182件の閲覧回数
Smiffytech
Contributor III

THIS WORKS! Thank you!

So - what do I change to stop Processor Expert from constantly regenerating that file with the L rather than the l?

0 件の賞賛
返信
11,181件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

as CodeWarrior V10.3 is not supported for Linux now I see two workarounds:

#1

Create new Limits.h as copy of the existing limits.h file in (./CodeWarrior_MCU_10.2/MCU/lib/hc08c/include/)


#2

or freeze the generated code of EventCntr component and change it manually as was mentioned in my previous post.


best regards

Vojtech Filip

Processor Expert Support Team

11,181件の閲覧回数
Smiffytech
Contributor III

Many thanks - I think solution #1 is the way to work, as any future project will pick up the copy - assuming that freezing generated code will only work for current project.

I know that I can't go to 10.3 in Linux - sad though it is for me.  When working on my desktop machine, I run 10.3 in a Windows virtual machine. My laptop, however, isn't powerful enough for this, so for the HCS08 projects that I need to run between the two machines, I'm stuck with 10.2

Thanks again for this solution!

0 件の賞賛
返信