Asynchronical serial: unable to read values 0x00 with PE routine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Asynchronical serial: unable to read values 0x00 with PE routine

1,102件の閲覧回数
juanignaciotroi
Contributor III

Hello

With the KE02 on CW IDE I'm trying to implement an RS232 component using the asynchronical serial component provided with the processor expert.

Having had enabled interrupts, and within the ISR calling the function <AS1_RecvChar> - generated by the processor expert - I am able to read any type of character with the exception the character NULL (0x00). 

Is there any reason why this may happen? Could it be that the interrupt is never called when a NULL is on the Rx?

Kind regards, 

Juan Ignacio Troisi

0 件の賞賛
返信
1 返信

984件の閲覧回数
juanignaciotroi
Contributor III

Can anyone help me with this issue?

0 件の賞賛
返信