Adding LVDS Panel with Touch Controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding LVDS Panel with Touch Controller

2,919件の閲覧回数
JK-IMX
Contributor V

Hi NXP

There's a request that Customer would like to solve.

They're trying to add a LVDS panel w/ Touch controller of Synaptic S3385.

Could you please us with Porting Guide to enable device especially focusing on Touch controller part?

This is asked since the NXP' porting guide does not handle the touch controller related part now.

They would like to clarify how to modify dts file to support a new touch device which is connected to I2C1. The interrupt line is connected with GPIO1 as below figure.

Please let us know how to modify dts file to enable S3385 device driver which was provided by Synaptics. i2c and gpio for interrupt and something else. 

lvds_touch.png 

0 件の賞賛
返信
3 返答(返信)

2,839件の閲覧回数
JK-IMX
Contributor V

Hi Igor

Actually I am not able to get appropriate info from the boundary device examples. Hope to add touch I2C controller into Porting guide. 

Regards, 

Jack

0 件の賞賛
返信

2,900件の閲覧回数
JK-IMX
Contributor V

Thanks Igor for your kind reply.

0 件の賞賛
返信

2,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi James

 

unfortunately this part is not supported in nxp bsps, may be recommended to look

at boundary devices touch examples:

https://boundarydevices.com/tag/touch-screen/

https://www.digi.com/resources/documentation/digidocs/90002284/reference/bsp/v4-9-cc6_cc6qp/r_touch_...

 

Best regards
igor