Traces under Isolated Gate Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Traces under Isolated Gate Driver

跳至解决方案
4,029 次查看
travisalexander
NXP Employee
NXP Employee

Hey Travis,

Could you advise on this question?

 

I've seen that your competitors will state in their datasheets that no traces or planes should be placed underneath the isolation area. Is this also the case for the NXP part?

 

 

 

Jack Jamieson

M: (419) 261-5225

 

标签 (1)
0 项奖励
回复
1 解答
4,025 次查看
travisalexander
NXP Employee
NXP Employee

Hi Jack,

Yes this is the case--no traces under the IC.

The reason you can't have traces under the gate driver is to meet creepage and clearance isolation requirements separating the HV gate from the LV MCU side.

We put this information in the GD3100 app note (AN12357, section 9.1).

Regards,

Travis

在原帖中查看解决方案

0 项奖励
回复
1 回复
4,026 次查看
travisalexander
NXP Employee
NXP Employee

Hi Jack,

Yes this is the case--no traces under the IC.

The reason you can't have traces under the gate driver is to meet creepage and clearance isolation requirements separating the HV gate from the LV MCU side.

We put this information in the GD3100 app note (AN12357, section 9.1).

Regards,

Travis

0 项奖励
回复