Short circuit test using Flex GUI with FRDMGD3160XM3EVM evaluation board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Short circuit test using Flex GUI with FRDMGD3160XM3EVM evaluation board

2,380 次查看
AmerKarout
Contributor II

Hello Everyone,

 

I am currently using the FRDMGD3160XM3EVM evaluation board along with flex GUI to do a short circuit test on the XM3 module. I wonder what specific register I should configure to do the test.

I know that I should disable the DESAT, Is there any other thing I should do to protect the gate drive if the DUT fails? 

标签 (2)
0 项奖励
回复
3 回复数

2,345 次查看
guoweisun
NXP TechSupport
NXP TechSupport

For the 2LTO and SSD setting value which need IGBT/SIC vendor provide, GD3160 can't decide this parameters, you should communicate with vendor of SIC/IGBT then configure it into GD3160.

 

0 项奖励
回复

2,341 次查看
AmerKarout
Contributor II
Hi Guoweisun,

Thanks for your reply. My question is not about how to configure 2LTO or SSD. I am doing a short circuit test and those two things are disabled completely during this test. My question (is there any other registers I should configure while I am doing short circuit test ???)

regards,
Amer
0 项奖励
回复

2,329 次查看
guoweisun
NXP TechSupport
NXP TechSupport

For the short test you should get the SIC short parameters then use GD3160 to execute. Actual it depend on the request of SIC.

0 项奖励
回复