Short circuit test using Flex GUI with FRDMGD3160XM3EVM evaluation board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Short circuit test using Flex GUI with FRDMGD3160XM3EVM evaluation board

2,384 Views
AmerKarout
Contributor II

Hello Everyone,

 

I am currently using the FRDMGD3160XM3EVM evaluation board along with flex GUI to do a short circuit test on the XM3 module. I wonder what specific register I should configure to do the test.

I know that I should disable the DESAT, Is there any other thing I should do to protect the gate drive if the DUT fails? 

Labels (2)
0 Kudos
Reply
3 Replies

2,349 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the 2LTO and SSD setting value which need IGBT/SIC vendor provide, GD3160 can't decide this parameters, you should communicate with vendor of SIC/IGBT then configure it into GD3160.

 

0 Kudos
Reply

2,345 Views
AmerKarout
Contributor II
Hi Guoweisun,

Thanks for your reply. My question is not about how to configure 2LTO or SSD. I am doing a short circuit test and those two things are disabled completely during this test. My question (is there any other registers I should configure while I am doing short circuit test ???)

regards,
Amer
0 Kudos
Reply

2,333 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the short test you should get the SIC short parameters then use GD3160 to execute. Actual it depend on the request of SIC.

0 Kudos
Reply