Merging 2 different sdk samples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Merging 2 different sdk samples

2,106 Views
Asimoes
Contributor II

Im doing a PMSM control and im using a FRDM-MCXN947  , so im willing to do the motoro control with AI but i have the motor control sample and ai sample. I dont have idea if i can merge two different sdk samples in the same project and make it work in the card as the same project. Also about the PSMS sdk example the FreeMASTER programm is capable of create a database to train the AI ML model.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,096 Views
RafaR
NXP Employee
NXP Employee

Hello Asimoes

In this part of the community we provide support to other PNs, I recommend that you go to MCX Microcontrollers, so that my colleagues can see your case and help you.

Enjoy your weekend

Have a great day and best of luck.

0 Kudos
Reply