MM9Z1J638BM2EP Part ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1J638BM2EP Part ID

Jump to solution
3,359 Views
hilodavid
Contributor II

Dear Experts,

因我們在Document Number: MM9Z1_638D1 (Rev. 5.0, 11/2016)文件內, 找不到MM9Z1J638BM2EP這顆IC的Part ID, 還請幫忙解答, 謝謝你~

BTW, 但在MC9S12ZVM系列的文件內, 就能找到其他相關IC的Part ID說明,

例如: MC9S12ZVMC256, Mask Set Number: 0N00R, Part ID: 0x00180000, Option: CAN

         MC9S12ZVMC256, Mask Set Number: 1N00R, Part ID: 0x00180100, Option: CAN

         MC9S12ZVML12, Mask Set Number: N06E, Part ID: 0x00170000, Option: LIN

 

Best Regards,

David

Labels (1)
0 Kudos
Reply
1 Solution
3,325 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @hilodavid,

Unlike S12ZVM that mentioned, the MM9Z1_638 parts have just one ID:

0x02070207   (2N27G)

I think this is why it is not specified in the datasheet.

 

Best regards,

Daniel

View solution in original post

0 Kudos
Reply
3 Replies
3,314 Views
hilodavid
Contributor II

Dear Daniel,

Yes, it is already solved because we read the part ID is indeed 0x02070207.

Thank you very much!

Best Regards,

David

3,317 Views
hilodavid
Contributor II

Dear Daniel,

Thanks for the help, the read is indeed 0x02070207.

 

Best Regards,

David

0 Kudos
Reply
3,326 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @hilodavid,

Unlike S12ZVM that mentioned, the MM9Z1_638 parts have just one ID:

0x02070207   (2N27G)

I think this is why it is not specified in the datasheet.

 

Best regards,

Daniel

0 Kudos
Reply