MM9Z1J638BM2EP Part ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1J638BM2EP Part ID

ソリューションへジャンプ
3,373件の閲覧回数
hilodavid
Contributor II

Dear Experts,

因我們在Document Number: MM9Z1_638D1 (Rev. 5.0, 11/2016)文件內, 找不到MM9Z1J638BM2EP這顆IC的Part ID, 還請幫忙解答, 謝謝你~

BTW, 但在MC9S12ZVM系列的文件內, 就能找到其他相關IC的Part ID說明,

例如: MC9S12ZVMC256, Mask Set Number: 0N00R, Part ID: 0x00180000, Option: CAN

         MC9S12ZVMC256, Mask Set Number: 1N00R, Part ID: 0x00180100, Option: CAN

         MC9S12ZVML12, Mask Set Number: N06E, Part ID: 0x00170000, Option: LIN

 

Best Regards,

David

ラベル(1)
0 件の賞賛
返信
1 解決策
3,339件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @hilodavid,

Unlike S12ZVM that mentioned, the MM9Z1_638 parts have just one ID:

0x02070207   (2N27G)

I think this is why it is not specified in the datasheet.

 

Best regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,328件の閲覧回数
hilodavid
Contributor II

Dear Daniel,

Yes, it is already solved because we read the part ID is indeed 0x02070207.

Thank you very much!

Best Regards,

David

3,331件の閲覧回数
hilodavid
Contributor II

Dear Daniel,

Thanks for the help, the read is indeed 0x02070207.

 

Best Regards,

David

0 件の賞賛
返信
3,340件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @hilodavid,

Unlike S12ZVM that mentioned, the MM9Z1_638 parts have just one ID:

0x02070207   (2N27G)

I think this is why it is not specified in the datasheet.

 

Best regards,

Daniel

0 件の賞賛
返信