H Bridge 24V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

H Bridge 24V

3,787件の閲覧回数
lwalus
Contributor I

In one of my projects i need to use H Bridge to control Electronic Throttle and Solenoids in 24V battery system. Actually all integrated H Bridges heve recommended supply voltage up to 28V. There are small saefty margin.

What is recommended solution for 24V Battery Systems? Maybe 28V is enough?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

3,777件の閲覧回数
lwalus
Contributor I

OK, but in automotive during charging it could be about 28V (likne maximum volotage for NORMAL operation). This parts are normally used for example in trucks?

0 件の賞賛
返信

3,767件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Łukasz,

unfortunately we do not have a designed a H-bridge driver specifically for the 24V applications. Although the mentioned can be used in the 24V application, you need to make sure, that the operating conditions will be not exceeded for proper operation and that the maximum values are not exceeded in order not to damage the component. These parts are usually used in 12V applications. 

I have picked for you devices from our powertrain and engine control portfolio, which are designed and recommended for the 24V applications. Please check them.

MC33PT2001 MC33PT2000 MC33937 MC33816 

The MC33816 is a solenoid controller, perhaps this one will be suitable for your application?

JozefKozon_0-1653396074176.png

With Best Regards,

Jozef

0 件の賞賛
返信

3,779件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Łukasz,

please see this link for our H-bridge portfolio. The MC33HB2000, HB2001, HB2002 and the MC33926 can be used in 24V systems.  

JozefKozon_0-1653392803730.pngJozefKozon_1-1653392833966.png

We also have additional Powertrain and Engine Control ICs. Please see this link. 

With Best Regards,

Jozef

 

0 件の賞賛
返信