GD3160-FAILSAFE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GD3160-FAILSAFE

1,993 Views
irbaz7
Contributor I

In half bridge configuration , there are 6 GD3160 corresponding to 6 SiC. Through a externally connected BJT to 5V, FSENB pin of each of the 6 GD3160 is pulled to High(the FSENB pin of each of the gate driver are individually connected to 5V) and FSSTATE pin is pulled low (for all 6 GD3160).

If due to a permanent failure, a BJT stops conducting which is connected to the FSENB pin of a gate driver i and it result in FSENB pin low of the corresponding gate driver therefore its Gate (GH) is pulled low but the other 5 gate driver are functioning normally.

Labels (1)
0 Kudos
Reply
1 Reply

1,975 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI irbaz7

Thanks for your interest in NXP products.

So what's your questions for the GD3160 here?

 

 

BR

0 Kudos
Reply