syntax error at line one

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

syntax error at line one

1,816 Views
maheshwarreddy
Contributor I

we are using the code warrior  v8.8 in that while entering into debug that time we are getting an error .tha errors ccs log will be attached below .

Thank you

Best regards

Maheshwar reddy.

Tags (2)
0 Kudos
Reply
1 Reply

1,714 Views
Pavel
NXP Employee
NXP Employee

Test your connection of your TAP to the board.

Use /Tools/Hardware Diagnostics menu of CodeWarrior 8.8.

The MPC866 uses BDM connection (10pins) for debugging.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply