Hi guys.
I have a dozen non-working devices, after bad developers,
the developers forgot to run chkdsk/fsck at startup.
and after problem with R/W FS, device stop work.
...I have already encountered/repair this case for other vendor too,
so, now these devices don't work.
and i want to fix this error with JTAG.
fixing the file system and writing back.
(yes I know from Bad Block, ECC, Spare and etc
also, I don't have a root password for device,
and there isn't uboot on the device)
so, I have
1) MPC8321 (MPC8323E.pdf)
2) S29GL064N at CS0
3) MT29F2G16 at CS1 - NAND !!!
4) TRACE32 unit with MPC82xx/83xx adapter.
I read S29GL064N via TRACE32/MPC8321, no intresting inside.
but I can't read MT29F2G16 in any way.
I initialize the MPC8321, just as it looks in the bootloader,
Data.Set ANC: IOBASE () + 0x05008 %Long 0x70001081; LBC_BR1
Data.Set ANC: IOBASE () + 0x0500C %Long 0xFFFF8100; LBC_OR1
Data.Set ANC: IOBASE () + 0x00028 %Long 0x70000000; LB_LAWBAR1
Data.Set ANC: IOBASE () + 0x0002C %Long 0x8000000B; LB_LAWAR1
then try
FLASHFILE.CONFIG IOBASE () + 0x05000 0x0 0x70000000 1
FLASHFILE.TARGET 0x00001000 +0x1fff 0x00003000++0x1FFF nand2g16_ppcpq.bin
but that doesn't help me, I get the error "warning: function not implemented"
I tried different options, but I can't understood what the problem was ((
also, as you can imagine, I haven't support for T32 ))
so I wanted to ask other developers,
maybe someone can help me with TRACE32 config,
or another budget solution, for flash MT29F2G16 via mpc8321 and jtag.
thanks.
You could use CodeWarrior for PA 10.5.1 + CodeWarrior TAP.
For flash programming/dumping, please refer to the application note https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flash-Programmer-for-CodeWarrior-Power-Ar... please add and execute the "Dump Flash actions" in PA Flash Programmer Task panel.
In CodeWarrior IDE, please create a bare board project for MPC8323 processor, please select flash device MT29F2G8 in the flash device list.
You could download CodeWarrior 10.5.1 from the following link.
https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing
You could purchase CodeWarrior TAP from the following link.
as I understand from goofle and mtd, there are different ways to connect NAND .
1) fsl_elbc_nand.c
2) fsl_ifc_nand.c
3) fsl_upm.c
8323 support only UPM,
and CW for PA and CW TAP only has Flash_Programmer\EPPC\
MT29FxG08-eLBC.elf and MT29FxG08-IFC.elf .
so, for 8323 I need found bootloader for UPM or am I wrong ?
my DTS file received from the bootflash
localbus@ff405000 {
#address-cells = <0x01>;
#size-cells = <0x01>;
compatible = "fsl,mpc8321-localbus\0fsl,pq2pro-localbus";
reg = <0xff405000 0xd8>;
ranges = <0x00 0x70000000 0x01>;
nand-flash@0 {
compatible = "Micron MT29F2G16ABA\0fsl,upm-nand";
reg = <0x00 0x01>;
width = <0x02>;
upm = [41 00];
upm-cmd-offset = <0x08>;
upm-addr-offset = <0x10>;
gpios = <0x02 0x0f 0x00>;
wait-pattern;
wait-write;
chip-delay = <0x64>;
};
};
thanks for answer, i try order CodeWarrior TAP,
1) but I need 3 week for delivery,
2) and I'm not sure if 29F2G16 will be read with 29F2G08 config,
3) also in CW SW, all NAND with the "-eLBC" remark,
I see eLBC when mpc8313 is connected to T32.
but on mpc8321/mpc8323 - in T32, i see only LBC.
I see that the simple commands, for working with NAND,
like read nand ID, use the addresses
IOBASE()+0x5068
IOBASE()+0x5070
I can probably write the Flash script myrself,
but it's difficult for me