please find the attachment and clarify the doubt...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

please find the attachment and clarify the doubt...

1,045 Views
lakshmit
Contributor I

i have attache my requirement,kindly read this and reply to me.

0 Kudos
Reply
2 Replies

961 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> During these transaction, whether,core will stop its normal

> cycle and reads the port data and writes to DDR2? /is core

> intervention required to write PCIe data to DDR2 or not?.

The core operation will not be interrupted - i.e. PCI Express transactions targeting MPC8548 inbound ATMU with translation to DDR2 SDRAM region are converted to direct memory write operations by the PCI Express interface.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

961 Views
lakshmit
Contributor I

Thanks

Regards

Lakshmi T,Scientist 'E'

DARE

bangalore

-- Original Message --

0 Kudos
Reply