pl provide me command sequence to test I2C interface.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pl provide me command sequence to test I2C interface.

1,916 Views
ranjeetsinha
Contributor I

i have to configure MPC8548 as I2C master. I want to test it at 100Kbps.

pl provide me command sequence.

0 Kudos
Reply
2 Replies

1,789 Views
andymastronardi
NXP Employee
NXP Employee

Ranjeet,

please see attached.

Andy

0 Kudos
Reply

1,787 Views
Pavel
NXP Employee
NXP Employee

See attached file. It is simple program I2C example for the MPC8548. It is CodeWarrior 9.8 project for the MPC8548CDS board.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply