mtmsr[fp] do not follow sync

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mtmsr[fp] do not follow sync

1,239件の閲覧回数
poloyellow
Contributor I

hi,

   I had a test in mpc8640.  I try to do mtmsr[fp] but forget the synchronizing instruction followed.

for example:

/****************************************/

mfmsr  r3

rlwinm r3,r3,0,19,17     /*mask  fp*/

ori  r3,r3,0x1000   /* set ME*/

mtmsr  r3

sync

ori  r3,r3,0x2000   /* set fp, without sync followed*/

mtmsr  r3

stfd  f0,  48(r1)

/*********************************/

When I excute the code, the cpu seems do not enter any exception or interrupt, include machine check, and there isn't any response in serial port. So I don't know what the cpu is doing after the instruction 'stfd', and which state the cpu is in.

Can anyone give me any explanation?

 Thanks.

Polo Yellow

タグ(1)
0 件の賞賛
返信
1 返信

1,139件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

According to E600 Core Reference Manual:

"A context synchronizing instruction must follow an mtmsr instruction"

This is said explicitly in section Section 2.1.4.4 "Machine State Register (MSR)"

In this statement word "must", as per my personal understanding, means that violating this rule will lead to unpredictable results.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信