choose powerPC main frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

choose powerPC main frequency

1,116件の閲覧回数
jeffcao
Contributor I

I want to Know the relationship between the main frequency of MCU and the transmission bandwidth.

I don't know how to choose the main frequency of the chip.I need to achieve a balance between the main frequency and the power consumption.

ラベル(1)
0 件の賞賛
返信
1 返信

957件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

I do not see what particular PowerPC chip and transmission type you mean. Typically if there is such  restriction then device reference manual describes that. For example the MPC8548e manuals says: For proper PCI Express operation, the CCB clock frequency must be greater than (500MHz)*(PCI Express link width) /8

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信