mpc860 Powerquicc processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc860 Powerquicc processor

1,564 Views
ravadasrikanth3
Contributor I

I'm using mpc860 Powerquicc processor with 66mhz clock ,as per my observations Hreset and Sreset are toggling clock pulse width is 8us ,actually it is new board code is not flashed in to it.

can anyone tell us why these pins are toggling  ?

Tags (1)
0 Kudos
Reply
1 Reply

1,497 Views
Bulat
NXP Employee
NXP Employee

Most probably it happens due to the watchdog timer which is enabled after reset, see description of the System Protection Control Register (SYPCR).

Regards,

Bulat

0 Kudos
Reply