Example work with DMA on mpc8308

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example work with DMA on mpc8308

1,906件の閲覧回数
nambuluseddie
Contributor I

Good day.

My company bought several modules with mpc8308 on board. But following the documentation, we did not manage to implement DMA data transfer. Is it possible to get an example of the implementation of data transfer over DMA?

Regards Eddie.

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,811件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no DMA example for the MPC8308, but is possible to refer to the Linux DMA driver source code:

linux/mpc512x_dma.c at master · torvalds/linux · GitHub 

0 件の賞賛
返信

1,811件の閲覧回数
nambuluseddie
Contributor I

Yes, i saw it. But i don't know how to use it in MPC8308. In documentation i looked for sample for use DMA, but it is not full. Can you give me a little full sample for just transfer some data by dma on mpc8308. I crying need it. Need support from NXP.

0 件の賞賛
返信