Hi,
We got a rapidio host and several rapidio agents connected via back plane, the host has trouble in discovering agent, and it's figured out that the host has enumerated the agent when the agent is in bootloader stage, and when the agent os is loaded, the host can no longer enumerate it again thus failed to send/recv messages to the agent. One solution we can image is to disable rapidio port when the agent is in bootloader assembly stage and re-enable it when os is up. Unfortunately, we never succeed. The assembly code in bootloader is as follows:
#define PmCCSR_0 (CCSRBAR + 0xC015C)
lis r8, HI(PmCCSR_0)
ori r8, r8, LO(PmCCSR_0)
lwz r7, 0(r8)
lis r9, HI(0x00800000)
ori r9, r9, LO(0x00800000)
ori r7, r7, r9
stw r7, 0(r8)
sync
The purpose is to set Port m Control Command and Status Register (PmCCSR) bit 8 to 1, but when we read this register in bootloader command line, the value never changed. we tried many place where to insert the assembly snippet in, both at the very beginning or when CCSR relocated and TLB set up. Am I doing anything wrong? Please help and thanks in advance!
Regards
Jia
已解决! 转到解答。
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		PORBMSR[HA]=001 AND PmCCSR[PD]=1 to disable port 1 to disable port1.
You also can disable the serdes lane using GUT_SRDSCR2 register.
Also, there's mistake in the assembly code that made it failed to set the corresponding register correctly.
#define PmCCSR_0 (CCSRBAR + 0xC015C)
lis r8, HI(PmCCSR_0)
ori r8, r8, LO(PmCCSR_0)
lwz r7, 0(r8)
#lis r9, HI(0x00800000)
#ori r9, r9, LO(0x00800000)
#ori r7, r7, r9 /* using ori here is wrong!! */
oris r7, r7, HI(0x00800000) /* should be corrected like this */
stw r7, 0(r8)
sync
Thanks
Jia
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		So, at reset setting PmCCSR[OPE] = 0. By doing this they hit the errata SRIO-A004"1. MAINT packet gets queued, but not sent.""The impact section of the errata clearly states that"outbound maintenance request packets will not be transmitted"and inbound maintenance packets may not be responded to.
 When PmCCSR[OPE]= 0
 - Inbound non-maintenance request packets may be responded to.- If the device configuration allows outbound requests to be pending in the controller, inbound maintenance request packets may not be responded to.- Outbound maintenance request packets will not be transmitted.
 My recommendation is to set PmCCSR[OPE]= 1. There are no plans to fix this issue.
Hi Yiping,
Thanks for your quick reply! As I mentioned, we want to disable rapidio ports in bootloader stage and enable it when os is up, in order to make it not discovered by rio host when in bootloader stage, otherwise the rio host wouldn't re-discovered it again when the agent os is up. So I've tried to set PmCCSR[PD] (Port Disable) to 1, not PmCCSR[OPE]. Unfortunately, I never succeed in setting PmCCSR[PD] to 1 in bootloader assembly code. I've even tried altering it under bootloader command line, but still failed. So, I would like to ask whether or not does my approach work or do I miss something?
Thanks
Jia