mpc8360 risc timer clocking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc8360 risc timer clocking

3,824 Views
eric2013
Fresh Out Contributor

In QEIWRM - 5.10.5 Timer Functional Description:

The clock input to the timer prescaler can be selected from the following sources:

• The system clock (ipg_clock)

• The system ‘slow go’ clock (ipg_clock internally divided by 16)

What does the "system clock" mean? Is it csb_clk, or ce_clk, or core_clk, or the PCI_CLK ( CLKIN not used)?

Thanks.

Labels (1)
0 Kudos
Reply
4 Replies

3,534 Views
LPP
NXP Employee
NXP Employee

ipg_clock is global IP clock. In case of MPC8360, ipg_clock = csb_clk

0 Kudos
Reply

3,534 Views
eric2013
Fresh Out Contributor

Thanks. But I got one different answer from Technical Support that  the "ipg_clock = one half of the QUICC Engine frequency" and the "QUICC Engine frequency" is the ce_clk.

0 Kudos
Reply

3,534 Views
LPP
NXP Employee
NXP Employee

You are right. The link is QEIWRM Rev. 4.4, section 5.10.2.2 GTM Clock Source Modes.

Please accept my apology for this inconsistence.

0 Kudos
Reply

3,529 Views
eric2013
Fresh Out Contributor

Thanks,LPP.

0 Kudos
Reply