mpc8360 risc timer clocking

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc8360 risc timer clocking

3,675 次查看
eric2013
Contributor I

In QEIWRM - 5.10.5 Timer Functional Description:

The clock input to the timer prescaler can be selected from the following sources:

• The system clock (ipg_clock)

• The system ‘slow go’ clock (ipg_clock internally divided by 16)

What does the "system clock" mean? Is it csb_clk, or ce_clk, or core_clk, or the PCI_CLK ( CLKIN not used)?

Thanks.

标签 (1)
0 项奖励
回复
4 回复数

3,385 次查看
LPP
NXP Employee
NXP Employee

ipg_clock is global IP clock. In case of MPC8360, ipg_clock = csb_clk

0 项奖励
回复

3,385 次查看
eric2013
Contributor I

Thanks. But I got one different answer from Technical Support that  the "ipg_clock = one half of the QUICC Engine frequency" and the "QUICC Engine frequency" is the ce_clk.

0 项奖励
回复

3,385 次查看
LPP
NXP Employee
NXP Employee

You are right. The link is QEIWRM Rev. 4.4, section 5.10.2.2 GTM Clock Source Modes.

Please accept my apology for this inconsistence.

0 项奖励
回复

3,380 次查看
eric2013
Contributor I

Thanks,LPP.

0 项奖励
回复