mpc8308 u-boot configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc8308 u-boot configuration

1,441 Views
zhoumr
Contributor I

Hi all:

   How to change mpc8308 u-boot configuration to support my board,hardware such as:

DDR:H5PS1G63JFR-S5C(64Mx16), 2chips

NOR FLASH:MX29GL512F(32Mx16),1chips

NAND FLASH:none

UART:SP3232EBCH

Default configuration just support 128M DDR,8M nor flash。Start with Nand flash。But I want the board start with nor flash。

The uboot version is u-boot-2009.11-rc1。

Thanks。

Tags (3)
0 Kudos
Reply
2 Replies

1,180 Views
ufedor
NXP Employee
NXP Employee

You could refer to the MPC8308RDB.h using the following link:

Cross Reference: /denx/u-boot/include/configs/MPC8308RDB.h 

It already has NOR Flash boot setting in the "#define CONFIG_SYS_HRCW_HIGH":

    HRCWH_ROM_LOC_LOCAL_16BIT |\
    HRCWH_RL_EXT_LEGACY |\

DDR changes:

#define CONFIG_SYS_DDR_SIZE        256 /* MB */
#define CONFIG_SYS_DDR_CS0_BNDS    0x0000000F

NOR Flash changes:

#define CONFIG_SYS_FLASH_BASE        0xFC000000 /* FLASH base address */
#define CONFIG_SYS_FLASH_SIZE        64 /* FLASH size is 64M */

/* 512 128KB sectors per device */
#define CONFIG_SYS_MAX_FLASH_SECT    512

NAND Flash change:

Remove NAND Flash parameters

0 Kudos
Reply

1,180 Views
zhoumr
Contributor I

Hi ufedor

Thank you help me!

But my board still can not boot.

Maybe "Memory Map" is incorrect.

My colleague use vxworks boot can work good, but only detect 128M DDR and 8M nor flash.

God, this web page hard to access from china.

WuHan, China, zhoumr. Thank you for your help!

0 Kudos
Reply