mpc8306 DDR2 timing reg setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc8306 DDR2 timing reg setup

1,320 次查看
go777
Contributor I

mpc8306 ddr2 setup:

RCWLR = 0x4423_0086;  input sys_clk = 33.333Mhz

so:

csb_clk = 133Mhz, DDR2_clk = 266Mhz

DDR2_tclk = 7.5ns

DDR2 Chip on MPC8306SOM is MT47H64M16HR-3,from micron's datasheet

tRP(min) = 15ns;

tRAS(min) = 40ns;

tRCD(min) = 15ns;

tRFC(min) = 127.5ns;

tWR(min) = 15ns;

tRCD(min) = 15ns;

tRRD(min) = 10ns;

tWTR(min) = 7.5ns;

by MPC8306 RefrenceManual:

DDR2_Timing_cfg_1_reg:

PRETOACT(tRP) =  15ns/7.5ns = 2;

ACTTOPRE(tRAS) = 40ns/7.5ns = 6;

ACTTORW(tRCD) = 15ns/7.5ns = 2;

CASLAT(CL) = 5;    CL = 3 clocks;

REFREC(tRFC) = 127.5ns/7.5ns -8 = 9;

WRREC(tWR) = 15ns/7.5ns = 2;

ACTTOACT(tRRD) = 10ns/7.5ns = 2;

WRTORD(tWTR) = 7.5ns/7.5ns = 1;

so, value of  DDR2_Timing_cfg_1 should be:

# TIMING_CONFIG_1

# bit 1-3 = 2 - PRETOACT precharge activate interval 3 clock cycles

# bit 4-7 = 6 - ACTTOPRE activate to precharge interval 9 clock cycles

# bit 9-11 = 2 = ACTTORW activate to r/w interval 3 clock cycles

# bit 13 - 15 = 5 - CASLAT CAS latency 3 clock cycles

# bit 16 - 19 = 9 - REFREC refresh recovery time 17 clock cycles

# bit 21 - 23 = 2 - WRREC data to precharge interval 3 clock cycles

# bit 25 - 27 = 2 - ACTTOACT activate to activate interval 2 clock cycles

# bit 29 - 31 = 1 - WRTORD write data to read command interval 2 clock cycles

#reg ${DDR_CONT_GROUP}TIMING_CFG_1 = 0x26259221

actually,the mpc8306som_init.tcl

# TIMING_CONFIG_1

# bit 1-3 = 3 - PRETOACT precharge activate interval 3 clock cycles

# bit 4-7 = 9 - ACTTOPRE activate to precharge interval 9 clock cycles

# bit 9-11 = 3 = ACTTORW activate to r/w interval 3 clock cycles

# bit 13 - 15 = 5 - CASLAT CAS latency 3 clock cycles

# bit 16 - 19 = d - REFREC refresh recovery time 21 clock cycles

# bit 21 - 23 = 3 - WRREC data to precharge interval 3 clock cycles

# bit 25 - 27 = 2 - ACTTOACT activate to activate interval 2 clock cycles

# bit 29 - 31 = 2 - WRTORD write data to read command interval 2 clock cycles

#reg ${DDR_CONT_GROUP}TIMING_CFG_1 = 0x3935d322

why?

the fact is use the value in mpc8306som_init.tcl is OK,use the value by calculate is wrong.

Have any suggestiton?

标签 (1)
0 项奖励
回复
1 回复

984 次查看
Bulat
NXP Employee
NXP Employee

It is possible that the problem happens due to WRTORD value, try to set it to 2.

We recommend that WRTORD value were set to 2 minimum, even if it is 1 as per SDRAM datasheet. See AN3369 app note for details.

Regards,

Bulat

0 项奖励
回复