ltib rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ltib rootfs

2,419件の閲覧回数
adeel
Contributor III

Hi,

I need to generate ltib jffs2 rootfs image. Could anybody send it to me? Or could anyone provide link to download latest LTIB image? The ltib image for mds board is not installable on my Ubuntu machine.

Thanks and regards,

Adeel

0 件の賞賛
返信
2 返答(返信)

2,023件の閲覧回数
hwrobel
NXP Employee
NXP Employee

Go to http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_BSP&tid=vanLINUX and select the correct BSP for whichever product or board you need it

Regards,

Heinz

0 件の賞賛
返信

2,023件の閲覧回数
adeel
Contributor III

I tried BSP for MPC85xx but it ended up in giving permission denied error while executing rpm command. I have setup visudo but it still shows error.

Could you please tell, can I use Systembuilder rootfs on MPC85xx platform?

Thanks and regards

Adeel

0 件の賞賛
返信