Hi Folks
We are using MPC8358E processor and we configured the local memory as shown in the fig.. mainly we are struggling with DDR interface. so please confirm this memory mapping.
is this DDR memory mapping is right?
Regards,
Venkat
Solved! Go to Solution.
Please refer to the MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual, 4.4.3 System Clock Domains:
"The internal ddr_clk frequency (for DDR) is determined by RCWL[DDRCM]. Note that the lb_clk clock
frequency (for Secondary DDR) is determined by RCWL[LBCM]. See Section 4.3.2.1, “Reset
Configuration Word Low Register (RCWLR).” Note that ddr_clk is not the external memory bus
frequency; ddr_clk passes through the DDR clock divider (÷2) to create the differential DDR memory bus
clock outputs (MCK and MCK). However, the data rate is the same frequency as ddr_clk."
Proposed memory map is incorrect.
Please read the MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual, 5.2 Local Memory Map Overview and Example
Thank you for replying,
As per MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual says, we can put boot flash on All zeros address or 0xFF80_0000 address. can you please elaborate more on this?. so that, my memory mapping is incorrect...
Regards,
Venkat
What is the DDR SDRAM size?
DDR size-64MB
Manfr- micron
What are RCWLR and RCWHR values?
You wrote:
> we are struggling with DDR interface
What does it mean?
RCWLR- 0x02230086
RCWHR- 0x00600000
You wrote:
> we are struggling with DDR interface
What does it mean?
#RCWLR Value :- 0x02230086
#LBCM-0 LBCM is equal to csb clk (266MHz)
#DDRCM-0 DDRCM is equal to csb clk (266MHz)
#SVCOD-00 system PLL VCO division is 4
#SPMF - 0010 system PLL multiplication factor is 2:1
#COREPLL -0100011 Core freq. 1600MHZ
#CEVCOD -10 QUIIC engine Freq. is 800MHZ
#CEPDF - 0 QUIIC Engine PLL div. factor is 0
#CEPMF- 00110 QUICC engine PLL mortification factor 6
#RCWHR Value :- 0x00600000
#PCIHOST-0 PCI is disable (not using)
#PCIARB-0 PCI arbiter is disable
#PCICKDRV - 0 PCI Buffers are disable
#COEDIS- 0 core can boot without waiting for config. by external master
#BMS- 0 boot memory space is all zeros to 0x007f_ffff
#BOOTSEQ- 00 boot sequencer disabled
#SWEN - 0 Software WDT disable
#ROMLOC- 110 local bus GPCM 16-bit ROM
#SDDRIOE -0 secondary DDR I/O disable
#TLE -0 big-endian mode
#LALE - 0 normal LALE timing
#LDP-0 initial value of SCIRL[LDP_A] is 1 means that LDP0-LDP3 are used for local data parity
You wrote:
> we are struggling with DDR interface
What does it mean?
> we are struggling with DDR interface
>What does it mean?
I am not able to access DDR memory. and DDR doesn't responding to the configured address.
There are two possibilities:
1) DDR SDRAM connection is incorrect
2) DDR controller initialization settings are incorrect.
Please provide:
1) DDR SDRAM connection schematics as searchable PDF
2) what is measured frequency of the MCK?
@ufedor are u there?
sir,
can we control DDR operating frequecy(MCK)? if it is yes! How?
Please refer to the MPC8360E PowerQUICC II Pro Integrated Communications Processor Family Reference Manual, 4.4.3 System Clock Domains:
"The internal ddr_clk frequency (for DDR) is determined by RCWL[DDRCM]. Note that the lb_clk clock
frequency (for Secondary DDR) is determined by RCWL[LBCM]. See Section 4.3.2.1, “Reset
Configuration Word Low Register (RCWLR).” Note that ddr_clk is not the external memory bus
frequency; ddr_clk passes through the DDR clock divider (÷2) to create the differential DDR memory bus
clock outputs (MCK and MCK). However, the data rate is the same frequency as ddr_clk."