issue with custom board Mpc8306

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

issue with custom board Mpc8306

817 Views
gangadhar1
Contributor I

I am using U-boot for booting and I am getting error on console as (ref :Freescale MPC8306SOM)

 


U-Boot 2010.06 (Sep 04 2018 - 14:46:02) MPC83XX

Reset Status: Check Stop, External/Internal Hard

CPU: e300c3, MPC8306E, Rev: 1.1 at 266.667 MHz, CSB: 133.333 MHz
Board: Freescale MPC8306SOM
I2C: ready
DRAM: 128 MiB
FLASH: 8 MiB
Firmware 'Microcode version 0.0.0 for MPC8306 r1.0' for 8306 V1.0
QE: uploading microcode 'Microcode for MPC8306 r1.0'
NAND: No NAND device found!!!
0 MiB
NIP: 00000004 XER: 00000000 LR: 07F9B4E4 REGS: 07ef6db0 TRAP: 0700 DAR: 00000000
MSR: 00083032 EE: 0 PR: 0 FP: 1 ME: 1 IR/DR: 11

GPR00: 00000000 07EF6EA0 07EF6F44 07FCE540 07EF7248 00000000 000C0000 0000000A
GPR08: 00001DB9 07FCE540 07FC8AAC 07EF9248 44000022 F7EFA7DF BFEAFFF3 09F79000
GPR16: EFFEFDFF E9DFFBFF EFFFFFFF EFFFFDFF 00001400 FFFFFFFF 00000000 07EF7248
GPR24: 000E0000 00000000 00000000 07FCE540 00000000 00800000 07FCC3A8 000C0000
Call backtrace:
FFFFFFED 07F9B6C0 07F9B7C4 07F9B4A8 07F7DA64 07F7C600
Program Check Exception
Resetting the board.

Can anyone suggest how to fix this issue..

0 Kudos
Reply
1 Reply

710 Views
Pavel
NXP Employee
NXP Employee

Program Check Exception reports about hardware problem on your board. Usually incorrect board initialization produces similar problem.

Check memory configuration, , NAND Flash enabling on your board.

Configuration of the u-boot is available in the following folder in u-boot source: /include/configs/.

 

See the following page:

https://en.wikipedia.org/wiki/Machine-check_exception


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply