codewarrior floating license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior floating license

971 Views
Irfan3
Contributor III

Hi Team,

I am using Codewarrior floating license from past 6-8 months. but from today i am facing this issue as mentioned below

lmgrd is not running: Cannot connect to license server system.
The license server manager (lmgrd) has not been started yet,
the wrong port@host or license file is being used, or the
port or hostname in the license file has been changed.
Server name: 10.60.101.136
License path: @10.60.101.136;
FlexNet Licensing error:-15,570

so, what could be the issue that can be causing this error. please provide help so that i can solve this issue.

 

thanks

irfan

0 Kudos
Reply
0 Replies