code warrior IDE v8.8 Error Unable to use the Plugin "EPPC - Debugger"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code warrior IDE v8.8 Error Unable to use the Plugin "EPPC - Debugger"

925件の閲覧回数
Abhi006
Contributor I

Hi,

I have an MPC8358E chip set. I installed Code Warrior v8.8 on Windows 10 (64-bit, 8 GB RAM). After installation, when I opened Code Warrior, I was unable to debug. I downloaded a valid license for Code Warrior and replaced it, but the issue persists. I also tried reinstalling Code Warrior multiple times, but the problem remains the same.

Here I have attached the screenshot for your reference

Screenshot (1).png

Thanks

0 件の賞賛
返信
4 返答(返信)

870件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The license file is invalid.

If you don't purchase CodeWarrior license, you could create an internal ticket from https://support.nxp.com/s/?language=en_US to require an evaluation license.

The put license.dat file in folder C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8.

0 件の賞賛
返信

848件の閲覧回数
Abhi006
Contributor I
I downloaded the license.dat and replaced it with the active one, but the problem persists. I have tried reinstalling Code Warrior 8.8 multiple times, but the issue remains. I am now receiving an error during installation (see attached screenshot for reference).

0 件の賞賛
返信

861件の閲覧回数
Abhi006
Contributor I

I downloaded the license.dat and replaced it with the active one, but the problem persists. I have tried reinstalling Code Warrior 8.8 multiple times, but the issue remains. I am now receiving an error during installation (see attached screenshot for reference).

Screenshot (5).png

0 件の賞賛
返信

711件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please ignore this installation error and continue to install Patch 8.8.6.

Because the latest CCS USB driver is included in Patch 8.8.6.

0 件の賞賛
返信