In case if you need just binaries for uloader ymodem download, than please use binaries that is in udisk in RDB board package. or you can build SDK/ASK, then there is uloader and barebox binaries as build result.
In case if you want to build a new uloader with ymodem support, than please refer to file, located at $barebox_root/arch/arm/lib/bootb.c.
It is a reference code on very old ASK release(ASK 3.0/3.1, which does not support barebox image header), your can use it as reference code and apply real code changes to new bootb.c
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------