What is the replacement or migration path for Users of the MPC875?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the replacement or migration path for Users of the MPC875?

1,473 Views
benl
Contributor I

I have recently been made aware of the the upcoming MPC875 End Of Life.   What is the suggested replacement or migration path for products that are still active and will remain active for some time to come?

0 Kudos
Reply
3 Replies

1,375 Views
Pavel
NXP Employee
NXP Employee
0 Kudos
Reply

1,375 Views
Pavel
NXP Employee
NXP Employee

See the AN2915.pdf Application Note:

https://www.nxp.com/docs/en/application-note/AN2915.pdf

 

This Application note contains information about migration from MPC82xx to MPC83xx.

It looks like that this Application Note can be used for your task.

 

Draw attention on the MPC8360 processor. The MPC8360 QE possibility is similar to the MPC875 CPM possibilities.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,375 Views
benl
Contributor I

Thanks Pavel for taking the time to answer my question.  

Some follow up questions:

The MPC875 is a PowerQUICC I processor, is there migration documentation from PowerQUICC to newer PowerQUICC II or PowerQUICC III?

Are all PowerQUICC I processors to be EOL'd next year?

thanks,

Ben

0 Kudos
Reply