What is the maximum capacity of MMC card we can connect to MPC8569?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the maximum capacity of MMC card we can connect to MPC8569?

1,867 次查看
ramchet
Contributor I

What is the maximum capacity of MMC card we can connect to MPC8569?

It's Reference manual ( MPC8569ERM Rev. 2  06/2011) mentions that it can support SDHC from 4GB to 32GB but what about the MMC size?

0 项奖励
回复
1 回复

1,392 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

The MPC8569 eSDHC is compatible with MultiMediaCard System Specification, Version 4.2 and SD Memory Card Specification, Version 2.0. The MMC spec. ver 4.2 does not specify maximal capacity in the block address mode. While the SD spec. ver. 2.0 specifies max card capacity. So in accordance to the MMC spec. ver 4.2 the MPC8569 supports MMC max capacity:
     2GB   -  Byte Address Mode
  > 2GB  -  Block Address Mode

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复