What can cause a code running on cpu 0 does not on cpu 1 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What can cause a code running on cpu 0 does not on cpu 1 ?

1,280件の閲覧回数
yasetoliva
Contributor I

The code is the FreeRTOS that I've built/run on the cpu0 of a twr-ls1021a board. I'm able to copy the code into ram and launch it from u-boot prompt. It works fine.

Then I run another code with cpu 0 to wake up the cpu 1 and put it running the FreeRTOS code. I can trace the execution of cpu 1 until the moment where the first task is to be started.  Then I don't know what's happening but the cpu 1 doesn't jump to the right address.

What can cause this bug? It's possible that it comes from the mmu, caches, etc enabled by u-boot on cpu 0 but NOT enabled on cpu 1?

Regards,

Yaset

0 件の賞賛
返信
2 返答(返信)

1,092件の閲覧回数
Pavel
NXP Employee
NXP Employee

Do you use an SMP version of FreeRTOS? See the following page:

https://sourceforge.net/p/freertos/discussion/382005/thread/b74e2952/

 

See also the following pages:

http://zedboard.org/content/freertos-running-both-arm-cores

 

and

 

http://www.rbccps.org/wp-content/uploads/2017/10/06961844.pdf

 

https://github.com/n-aizu/freertos-multicore

 

NXP offers Linux BSP for the TWR-LS1021a board:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

 

and

 

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

 

This BSP contains u-boot bootloader and Linux. The LS1021a CPU0 is enabled under u-boot and all cores are enabled under Linux.

Look at kernel code from this BSP about using all cores.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,092件の閲覧回数
yasetoliva
Contributor I

Thanks Pavel.

The problem was the timer that generate the ticks. We think, the timer is initialized during u-boot which is not executed by the cpu1. We have extracted the initialization code from the u-boot (u-boot-fslc/arch/arm/cpu/armv7/ls102xa/cpu.c) and included it in our code and it works now.

Thanks a lot for your answer.

Regards,

Yaset

0 件の賞賛
返信