We are studing to use a NAND Flash device in our design based in a MPC8306.
The NAND flash (128MB) will be connected to the eLBC and using the FCM mode. We plan to use a 16 bit port NAND, but in the reference manual is not clear if we can use this type of memory or only must use a 8 bit port NAND.
My question is: Could we use this 16 bit port NAND or should be replaced with a 8 bit port NAND?
Thank you for your help.
Manuel Ojea
 
					
				
		
 scottwood
		
			scottwood
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		16-bit NAND is not supported on this chip using FCM. See the documentation for BRn[PS], which says that 16-bit is only supported for GPCM and UPM.
It should be possible to connect a 16-bit NAND chip via UPM, but this is not straightforward and you would not have any hardware ECC. It is recommended that you use an 8-bit NAND chip, and stick with FCM. Also note that the NAND chip must not have pages that are larger than 2048 bytes.