UBoot compile and debug use CodeWarrior 8.8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UBoot compile and debug use CodeWarrior 8.8

ソリューションへジャンプ
4,311件の閲覧回数
00lirui
Contributor I

        Could i compile and debug uboot of mpc8306som code in CodeWarrior IDE  windows version?  How to do it? 

       Thanks.

0 件の賞賛
返信
1 解決策
4,037件の閲覧回数
catalindemergia
Contributor IV

Hi,

what you can do is to build on a Linux machine and after that import your ELF in CW

and attach to the board's u-boot to debug.

regards,

Catalin

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,036件の閲覧回数
lunminliang
NXP Employee
NXP Employee

For how to do, see this doc on community:CodeWarrior U-Boot Debugging

4,036件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section "Debugging the U-Boot Bootstrap Firmware" of the Pro & Linux App Edition Targeting Manual.pdf file. This file is available in the CodeWarrior folder.

4,038件の閲覧回数
catalindemergia
Contributor IV

Hi,

what you can do is to build on a Linux machine and after that import your ELF in CW

and attach to the board's u-boot to debug.

regards,

Catalin

0 件の賞賛
返信
4,036件の閲覧回数
00lirui
Contributor I

Do you mean I can debug code in windows  CW and compile on the linux machine?

0 件の賞賛
返信
4,036件の閲覧回数
catalindemergia
Contributor IV

yes, you can debug in CW running on a Windows machine the image that was built in Linux.

Catalin

0 件の賞賛
返信