U-Boot for PowerQUICC Based Designs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot for PowerQUICC Based Designs

1,687件の閲覧回数
stacym
Contributor I

I have found the app note (AN4173) that addresses customization of U-Boot for the i.MX51.  Is there a similar app note for the MPC8308 or the Power QUICC family of devices?  I am looking for some help in modifying U-Boot for some customized hardware.

Thanks!

タグ(1)
0 件の賞賛
返信
1 返信

1,501件の閲覧回数
lunminliang
NXP Employee
NXP Employee

I am not aware of that kind of document, there are two FTF presentation with the document number "FTF12-NET-F0180" and "FTF11-NET-F0399", they are talking about QorIQ P5 Processor, "Overcome the Challenges in Porting U-Boot and Linux OS", maybe your can refer to. The two presentation could be download from www.freescale.com.

0 件の賞賛
返信