TWR-P1025 board Memory Mapping structures?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-P1025 board Memory Mapping structures?

1,290件の閲覧回数
srihrsh29
Contributor I

I am trying to program Freescale Twr_p1025 board with the help of MULTI IDE. I am looking for the memory mapping structures of all the memory locations of the p1025 board. I went through the manuals but I do not see any helpful information. It would be great help if anyone can help me with the memory mapping and locations of the TWR_p1025 board. As I am trying to load the code in different memory locations?

0 件の賞賛
返信
1 返信

1,235件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

P1025 processor memory map is flexible and can be programmed. If you run your processor under debugger control, than memory map is programmed by debugger' target initialization file.

For more information please look P1025 Reference Manual, Chapter 2 "Memory map".

P1025 Reference Manual is available for download from P1025 Product Page, "Documentation" tab:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-pla...

0 件の賞賛
返信