TWR-P1025 board Memory Mapping structures?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-P1025 board Memory Mapping structures?

1,291 Views
srihrsh29
Contributor I

I am trying to program Freescale Twr_p1025 board with the help of MULTI IDE. I am looking for the memory mapping structures of all the memory locations of the p1025 board. I went through the manuals but I do not see any helpful information. It would be great help if anyone can help me with the memory mapping and locations of the TWR_p1025 board. As I am trying to load the code in different memory locations?

0 Kudos
Reply
1 Reply

1,236 Views
alexander_yakov
NXP Employee
NXP Employee

P1025 processor memory map is flexible and can be programmed. If you run your processor under debugger control, than memory map is programmed by debugger' target initialization file.

For more information please look P1025 Reference Manual, Chapter 2 "Memory map".

P1025 Reference Manual is available for download from P1025 Product Page, "Documentation" tab:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-pla...

0 Kudos
Reply